Electrical Floor Heating
News of current interest
> News Overview
> DEVI News
> Market News
> Press Releases
> News Archive
 
 
 
 
Electrical Floor Heating
Ice and snow melting systems from DEVI are designed to provide safety for buildings - and they can be installed in virtually any type of roof construction

DEVI’s feeling for snow

16 November 2009
When the winter sun melts the snow and ice, icicles start to form on the cold roof edges and gutters which over time can do a great deal of damage to the building and endanger vehicles and people passing by.

In order to avoid this and the manual work required to remove the ice, heating cables are installed in all drains such as gutter valleys, gutters, downpipes and eaves.

Optionally, heating cables are installed to melt the snow or slippery ice from ground areas.
News from DEVI

News

DEVI values an open and honest communication with all stakeholders.

We wish to enter into a factual and technical dialogue with consumers as well as professionals because we are convinced that openness encourage quality and strong results.